Plant SCADA Migration Information
This section contains the required and optional steps to migrate from pre-7.x versions of Plant SCADA to Power Operation.
NOTE: It is possible to restore and run the Citect project and includes on Power Operation and modify them to fully convert them to Power Operation projects. However, we recommend using the following migration steps to take advantage of the built-in power management features of Power Operation.
The required migration steps are:
- Create a New Project
- Import Citect Customizations
- Create Device Type Tags and Devices
- Export Alarm History
- Enable Waveforms
The optional migrations steps are: